CAP#.TRIGGER
Description
Selects which input will trigger the capture.
Examples
Usage
| Value | Description |
|---|---|
| 1-12 where 1 (default) | Digital Inputs DIN1 to 12 |
| 21-26 | Bidirectional digital inputs. DIO1 to 6 |
| 31-35 | Z-Pulses from feedbacks FB1 to 5 |
| 41-42 | Z-pulse from Axis 1 or 2 |
Not all drive models have the hardware to support all these options. For example, a single axis drive can not support 42.
Code
-->CAP1.TRIGGER 41 -->
Context
For more information please refer to Capture.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 12, 21 to 26, 31 to 35, 41 to 42 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics
Capture